Maybe you would like to know a little more about where our Cerabar pressure sensors and Ceraphant pressure switches are used in real life? As a matter of fact, these pressure sensors fit the process industry, whether close to the very heart of the processes or more towards utilities applications. Actually, one will find them e.g. in leakage detection control - for instance in compressed air networks, as well as in numerous tank level measurement applications where they are used in pairs to measure differential pressure. The same set up is also typical to monitor filters or pump performance. Many customers also use these sensors in the field of machine building, as well as to equip skids, particularly in the food and beverage industry. The scope of application is extremely wide as it extends to e.g. sprinkler systems, heating and ventilation installations and more. The following applications may not be the most typical, but they perfectly illustrate two major assets of our pressure sensors. The same dry ceramic measuring cell that equips both the Cerabar pressure sensor and the Ceraphant pressure switch equips thousands of dialysis pumps, knowing the very stringent accuracy and reliability requirements of medical equipment, this case illustrates the number one asset of our pressure sensors: their accuracy and their reliability. Cerabar pressure sensors have been used for pressure measurement in pilot emergency power generators using not less than airplane turbines, which says something about their robustness - another major asset of our E-direct series of instruments for pressure measurement.